FB#.BITS

Description

Specifies the number of BiSS sensor (position) bits for the BiSS encoder in use when used for linear motors. The required value for this parameter is provided by the feedback device manufacturer for the particular device being used.

Context

Only used for when FB#.MECHTYPE is linear and identified feedback is BiSS. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

position bits

Range

0 to 64

Default Value

26

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.BITS

3500h

06h

Unsigned16

-

-

Read/Write

No

FB2.BITS

3501h

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30400

1

30400 (0x76c0)

FB1.BITS

Unsigned16

Read/Write

Yes

30401

1

30401 (0x76c1)

FB2.BITS

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.BITS

30400

Unsigned16

Read/Write

-

FB2.BITS

30401

Unsigned16

Read/Write

-