Variable Table List

These are the modes when editing a variable in the Dictionary:

  • Cell: Only the selected cell is active. (Figure 1)
  • Figure 1: One active cell

  • Row: The entire row is active. (Figure 2)
  • Figure 2: Entire active row

Press the Spacebar to toggle the selection mode from cell to row.

See Table Keyboard Shortcuts.

When the selection mode is on cell, the variable editor enables you to enter each piece of information directly in the cell.

Double-click or press <Enter> to open the dialog box.

Use the mouse to drag the column separators in the main table header to resize the column widths.

Press these keys for browsing groups of variables:

Shortcut

Description

Ctrl + Page Up

Move the selection to the head of the previous group.

Ctrl + Page Down

Move the selection to the head of the following group.

For Table manipulation, see Windows Standard Conventions.

Concept Link IconSee Also