You are here: Annexes > List of KAS Literature > Installing KAS > Operational Procedures using the command line

Enhanced Write Filter Operational Procedures using the command line

Protect the PAC Image with EWF

The EWF should be activated on the PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system after the system is running and the PAC configuration is complete. If you want to change the CF image (such as a new KAS version or downloading a new application), then turn off the EWF filter, make the change, and then reactivate EWF.

  1. Open a command prompt by pressing Start > Run and type: cmd
  2. From the command prompt, type: ewfmgr C: -enable
  3. Reboot the PAC to activate the EWF

To ensure that the command has been entered correctly, execute the DOS command shell ewfmgr c: prior to rebooting the PAC. Check the field Boot Command, which should be set to "ENABLE", as seen in the image below.

Perform Changes on a Protected Volume

The EWF has to be disabled to perform changes on a PAC. After the changes are made the EWF is re-enabled.

  1. Open a command prompt by pressing Start > Run and type: cmd
  2. From the command prompt, type: ewfmgr C: -commitanddisable
  3. Reboot the PAC to commit the changes and disable EWF
  4. Make the desired changes (program installation, files record, etc.)
  5. From the command prompt, type: ewfmgr C: -enable
  6. Reboot the PAC to activate the EWF

Perform Small Changes on a Protected Volume

To commit changes without disabling and re-enabling EWF, a single commit can be commanded:

  1. From the command prompt, type: ewfmgr C: -commit
  2. Reboot the PAC to commit the changes (EWF remains active).

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™