| Component | Firmware Version | Download |
|---|---|---|
| 800MHz PDMM DriveControl device for regulating the speed, torque and position of a motor FW | AKD-M-MCEC-V1.15-00-003.i00 |
|
| 1.2GHz PDMM Drive FW | AKD-M-M1EC-V1.15-00-003.i00 |
|
To upgrade PDMM drive Firmware with KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger, continue from the previous procedure as follows:
Please note that the firmware download is limited to 16 drives at a time.
Give careful attention to any warning dialog that appears at this point. These warnings usually include important information about preventing damage to the drives.
|
Copyright © 2015 Kollmorgen™ |
|