You are here: Annexes > List of KAS Literature > Installing KAS > Related Documents

Introduction

This guide covers the main following procedures to have your KAS system up and running:

Related Documents

In addition to this Guide, you need the following manuals to install KAS

Title Description
AKD Quick Start Contains all information needed to safely install and setup an AKD drive
AKD Installation Manual Covers the most important points to install the drive hardware and software. Provides instructions for basic drive setup and connection to a network
AKD EtherCAT Communication Describes the installation, setup, and software protocol for the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs AKD product series

Alerts and Warnings

When alert symbols are seen in a manual, be alert to the potential for personal injury. Follow the recommended precautions and safe operating practices included with the alert symbols. Safety notices in the manuals provide important information. Read and be familiar with these instructions before attempting to install, operate, or perform maintenance. The purpose of this section is to alert users to possible safety hazards associated with equipments and the precautions that need to be taken to reduce the risk of personal injury and damage to the equipment. Failure to observe these precautions could result in serious bodily injury, damage to the equipment, or operational difficulty.

 

Related Documents

Alerts and Warnings


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™