You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisAddress

FunctionMLAxisAddressPipe Network motion icon

Description

Returns the motion bus address of the axis

Arguments

Input

ID

Description

ID name of the Axis Block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

OK

Description

Returns true when function successfully executes

 

Data type

BOOL

 

Unit

n/a

Default (.Q)

Description

Returns the motion bus address of the axis

 

Data type

DINT

 

Unit

n/a

Example

Structured Text

Axis1_Address := MLAxisAddress(PipeNetwork.AXIS1);

Ladder Diagram

Function Block Diagram

MLAxisAddress: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™