You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisGenIsEN

FunctionMLAxisGenIsENPipe Network motion icon

Description

Check if the internal TMP"Trapezoidal Motion Profile" This pipe block is a source block that frequently serves as a virtual master for a system composed of several pipes. Generally, a trapezoidal motion profile generator is used to generate a flow of values with a first derivative which produces a trapezoidal trajectory generator of the axis is enable. Returns TRUE if the internal generator is enabled.

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisGenIsRdy

Example

Structured Text

 

MLAxisGenIsEN(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisGenIsEN: LD example

 

Function Block Diagram

MLAxisGenIsEN: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™