You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisResetErrors

FunctionMLAxisResetErrorsPipe Network motion icon

Description

Clears errors of the specified axis

Arguments

Input

ID

Description

ID name of the Axis Block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Previous Function Name

MLAxisClrErrors

Example

Structured Text

 

MLAxisResetErrors( PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisResetErrors: LD example

Function Block Diagram

MLAxisResetErrors: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™