You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisWriteModPos

FunctionMLAxisWriteModPosPipe Network motion icon

Description

Set the value period of the axis. Returns TRUE if the function succeeded.

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

ModuloPosition

Description

Sets the Axis Period Value when Mode is set to Modulo.

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Example

Structured Text

 

MLAxisWriteModPos(PipeNetwork.Axis1, 360) ) ;

 

Ladder Diagram

MLAxisWriteModPos: LD example

Function Block Diagram

MLAxisWriteModPos: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™