You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisWritePos

FunctionMLAxisWritePosPipe Network motion icon

Description

Used to set a position offset at the Axis when the Pipe Network:

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Position

Description

Position offset.

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Previous Function Name

MLAxisSetZero

Example

Structured Text

 

MLAxisWritePos( PipeNetwork.Axis1, 0) ;

 

Ladder Diagram

MLAxisWritePos: LD example

Function Block Diagram

MLAxisWritePos: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™