You are here: Technical References > Motion Library > Motion/Pipe Network > Motion Library - Convertor

Motion Library - Convertor

Name Description Return type
MLCNVConnect Connects a converter Pipe Block to the specified axis BOOL
MLCNVConnectEx Connects an extra converter Pipe Block to the specified axis. This function connects the output of a pipe to an axis data other than the control position. BOOL
MLCNVDisconnect Disconnects a converter Pipe Block from its associated axis BOOL
MLCNVInit Initializes a converter Pipe Block in Position or Speed mode BOOL

 

MLCNVConnect

MLCNVConnectEx

MLCNVConECAT

MLCNVDisconnect

MLCNVInit


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™