You are here: Technical References > Motion Library > Motion Library - Common > Coordinated Motion - Motion

Coordinated Motion Motion Library

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Description
MC_AxisSetDefaults Sets the default kinematic parameters for an axis.
MC_GrpHalt Performs a controlled motion stop of all the axes in the group
MC_GrpSetOverride Sets the velocity factor that is multiplied to the commanded velocity of all axes in the group.
MC_MoveCircAbs Commands interpolated circular movement on an axes group to the specified absolute positions.
MC_MoveCircRel Commands interpolated circular movement on an axes group to the specified relative positions.
MC_MoveDirAbs Commands movement of an axes group to an absolute position regardless of path.
MC_MoveDirRel Commands movement of an axes group to a relative position regardless of path.
MC_MoveLinAbs Commands interpolated linear movement on an axes group to the specified absolute positions.
MC_MoveLinRel Commands interpolated linear movement on an axes group to the specified relative positions.

 

MC_AxisSetDefaults

MC_GrpHalt

MC_GrpSetOverride

MC_MoveCircAbs

MC_MoveCircRel

MC_MoveDirAbs

MC_MoveDirRel

MC_MoveLinAbs

MC_MoveLinRel


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™