You are here: Technical References > Fieldbus Library > EtherCAT Library > ECATWriteData

FunctionECATWriteDataPLCopen motion iconPipe Network motion icon

Description

Modify the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs process image by directly writing values in it.

If you have a device other than the drive, ECATWriteData is used for more than just debug. It is used to set the status of the module (e.g. Stepper I/O slice) in the case your project is based on an external XML"Extensible Markup Language " XML is a general-purpose markup language. It is classified as an extensible language because it allows its users to define their own tags file because it contains unsupported EtherCAT Device.

Arguments

Input

Offset Description Offset in bytes from the beginning of the frame
  Data type UINT
  Range 0 - 1500
  Unit bytes
  Default —
Nbytes Description Number of bytes to write
  Data type SINT
  Range 1, 2 or 4
  Unit bytes
  Default —
Value Description Value to be written in the image. Only the number of bytes specified by Nbytes is copied.
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit n/a
  Default —

Output

Default (.Q)

Description True if data was written

See more details here

  Data type BOOL
  Unit n/a

Related Functions

ECATReadData

Example

Structured Text

//For use with Kollmorgen Thermocouple slice I/O to read in deg C
//Lookup offset by exporting ENI file after EtherCAT network is scanned
//Use offst 124 (byte) to write 0 in control word to allow temperature to be shown on status byte

ON WriteControlOnly DO
ECATWriteData
( 124, 1, 0 );
END_DO

FBD

FFLD

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™