You are here: Technical References > Kollmorgen UDFBs > PLC > Pulse Width Duty Cycle

Function Block FB_PWDutyOutput

Description

The PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated Width Duty Cycle function block accepts an input value between the minimum and maximum input range and converts this to a duty cycle percentage. The output is then cycled on and off over the period of the duty cycle at the duty cycle percentage. If it is desired to have the output ON time range from 0 to the duty cycle period, the minimum should be set to zero and the maximum to the duty cycle period. If the calculated duty cycle based on the input and range values is less than the minimum ON time (MinTime), the output will not come on. If the calculated duty cycle is between or equal to the range values the output is cycled by the duty cycle. If the calculated duty cycle is greater than the maximum ON time (MaxTime) the output will remain on.

The following figure shows the function block I/O

UDFB PWDutyOutput

Figure 11-189: Pulse Width Duty Cycle

Arguments

Input

uEN01

Description

EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. for the block

 

Data type

BOOL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uInputCommand

Description

Duty Cycle Input (sometimes the output of a PID"Proportional-Integral-Derivative" A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems. An "error" occurs when an event or a disturbance triggers off a change in the process variable. A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly block).

 

Data type

REAL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uPeriod

Description

Period of the duty cycle

 

Data type

TIME

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uMaxInput

Description

Maximum value for the Input

 

Data type

REAL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uMinInput

Description

Minimum value for the Input

 

Data type

REAL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uMaxTime

Description

Maximum on time for the Output

 

Data type

TIME

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

uMinTime

Description

Minimum on time for the Output

 

Data type

TIME

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

Output

OK

Description

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is OK.

 

Data type

BOOL

 

Unit

n/a

TM1

Description

Duty cycle on time

 

Data type

TIME

 

Unit

n/a

DutyOutput

Description

Indicates if output is on or off

 

Data type

BOOL

 

Unit

n/a

Usage

Flash a warning light for operators.

Related Functions

Timers

Example

Structured Text

 

Inst_FB_PWDutyOutput( PWDuty_3_Switch, PWDuty_In3, PWDuty_3_Period, PWDuty_3_MaxInput, PWDuty_3_MinInput, PWDuty_3_MaxTime, PWDuty_3_MinTime);

PWDuty_3_OK:=Inst_FB_PWDutyOutput.OK;

PWDuty_3_Time:=Inst_FB_PWDutyOutput.TM1;

PWDuty_3_Output:=Inst_FB_PWDutyOutput.DutyOutput;

 

 

Ladder Diagram

UDFB PWDutyOutput: LD example

 

Function Block Diagram

UDFB PWDutyOutput: FBD example

 

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™