Depending upon the system used, paths to file locations may be defined as either absolute (C://dir1/file1) or relative paths (/dir1/file1). Not all systems handle all options, and the paths will vary depending upon the system.
| System | Absolute Paths | Relative Paths | Handling of Directories |
|---|---|---|---|
| PDMM or PCMM |
|
|
There is no support for creating directories on the controller. Any path provided to the function blocks, file1 for example, will be appended with the default userdata folder which is:/mount/flash/userdata |
| Simulator |
|
|
When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Simulator/Application/userdata |
| PAC |
|
|
When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Runtime/Application/userdata |
See Also:
|
Copyright © 2015 Kollmorgen™ |
|