You are here: Technical References > Motion Library > Motion/PLCopen > MC_CreateAxis

FunctionMC_CreateAxisPLCopen motion icon

Description

This function creates a PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Axis. A call to this function is automatically generated when the application is compiled, based on the data entered in the PLCopen Axis Data dialog.

MC_CreateAxis

Figure 11-118: MC_CreateAxis

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

En

Description

Requests to create a PLCopen axis

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

AxisName

Description

Axis name

 

Data type

STRING

 

Range

—

 

Unit

n/a

 

Default

—

BusInterface

Description

Bus interface identifier:

“EtherCATDriver” = EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs interface

“MSBusDriver” = KAS Simulator interface

 

Data type

STRING

 

Range

—

 

Unit

n/a

 

Default

—

BusAddress

Description

Address of the drive on the bus

 

Data type

DINT

 

Range

bus dependent

 

Unit

n/a

 

Default

—

AxisNumber

Description

Axis number

 

Data type

UINT

 

Range

[1,256]

 

Unit

n/a

 

Default

—

AxisType

Description

Axis type:

0 (MC_AXIS_TYPE_SERVO) denotes servo

1 (MC_AXIS_TYPE_DIGITIZING) denotes digitizing

2 (MC_AXIS_TYPE_VIRTUAL_SERVO) denotes virtual servo

 

Data type

USINT

 

Range

[0,1]

 

Unit

n/a

 

Default

—

UserUnits

Description

User unit portion of the user unit/feedback unit ratio

 

Data type

DINT

 

Range

[1,4294967296]

 

Unit

User unit

 

Default

—

FeedbackUnits

Description

Feedback unit portion of the user unit/feedback unit ratio

 

Data type

DINT

 

Range

[1,4294967296]

 

Unit

feedback units. Note: The FeedbackUnits input must be a power of 2. If input FeedbackUnits is not a power of two, the axis will not be created, and the OK output will be FALSE.

 

Default

—

Rollover

Description

Rollover position (0 = no rollover)

 

Data type

LREAL

 

Range

[0, 4294967296]

 

Unit

User unit

 

Default

—

UpdateRate

Description

Servo update rate

(0, 1, and 2 are reserved for future enhancements)

3 = 125 μsec

4 = 250 μsec

5 = 500 μsec

6 = 1 msec

7 = 2 msec

8 = 4 msec

9 = 8 msec

 

Data type

UINT

 

Range

[3,9]

 

Unit

n/a

 

Default

—

Output

OK

Description

Indicates the axis has been created

See more details here

 

Data type

BOOL

Example

Structured Text

(* MC_CreateAxis ST"Structured text"
A high-level language that is block structured and syntactically resembles Pascal Example *)
AxisName1 := 'PLCOpenAxis1';
BusName1 := 'EtherCATDriver';
BusAddress1 := 1001;
AxisNumber1 := 1;
AxisType1 := MC_AXIS_TYPE_SERVO;
UserUnits1 := 360;
FeedbackUnits1 := 1048576;
Rollover1 := 0;
UpdateRate1 := 3;
MC_CreateAxis(AxisName1, BusName1, BusAddress1, AxisNumber1, AxisType1, UserUnits1, FeedbackUnits1, Rollover1, UpdateRate1);

Function Block Diagram

Ladder Diagram

MC_CreateAxis: LD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™