You are here: Technical References > Motion Library > Motion/PLCopen > MC_MachRegist

Function BlockMC_MachRegistPLCopen motion icon

Description

This function block enables Mark-to-MachineThe complete assembly of all connected parts or devices, of which at least one is movable registration and can be used on any servo or digitizing axis and with any move type. It is most frequently used in master/slave applications.

Used with ... Effect
Non-slave moves Resets the axis position when a good mark is captured by the fast inputThe inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action.
Slave moves In addition to resetting the axis position, applies a compensation offset to correct for the difference between the target position and the measured position. This provides the ability to compensate for product or process inconsistencies providing a system that remains synchronized with no accumulated error and maintaining repeatable accuracy throughout the process.

Arguments

Input

En Description Rising edge of EN enables execution
  Data type

BOOL

  Range

0, 1

  Unit

n/a

  Default

—

Axis Description Axis whose position is used to determine a good mark.
  Data type Axis_Ref
  Range The range of .AXIS_NUM is [1,256]
  Unit n/a
  Default n/a
TriggerInput Description

Structure specifying the fast input. The structure elements are:
InputID INT

0 = Capture Engine 0

1 = Capture Engine 1

Range is [0,1]

For information on configuring the capture engines, refer to AKD Capture Engine Configuration.

Direction INT
1 = rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge, 2 = falling edge, 3 = NA, 4 = toggle between both, falling edge first, 5 = toggle between both, rising edge first, range = [1,5]

TrigID INT
Axis number of the fast input. Zero indicates this trigger axis is to be the same as the Axis input. range = [0,256]


  • TrigMode INT (TriggerInput.TrigMode) is not presently supported by this function. The TriggerInput.Mode may be supported in a future software version.
  Data type TRIGGER_REF
  Range  
  Unit  
  Default  
Distance Description This is the expected distance between good marks. Along with Tolerance and Ignore, this value is used to determine if the mark detected by the fast input is a good mark.
  Data type LREAL
  Range When converted to feedback units, the range is [-251,251-1]. This value must have the same sign as Ignore.
  Unit user units
  Default n/a
Tolerance Description This value specifies the distance, plus or minus, about Distance to determine if the mark detected by the fast input is a good mark.
  Data type LREAL
  Range When converted to feedback units, the range is [0 ,251-1]
  Unit user units
  Default n/a
Ignore Description This value specifies the distance after the previous good mark in which any detected marks are ignored.
  Data type LREAL
  Range When converted to feedback units, the range is [-251,251-1]. This value must have the same sign as Distance.
  Unit user units
  Default n/a
Target Description This is the target position. This position is compared to the actual position captured by the fast input to determine the amount of registration compensation to apply.
  Data type LREAL
  Range When converted to feedback units, the range is: 
  • [-251,251-1] if PosAxis' rollover value is zero
  • [0, PosAxis' Rollover Value] if PosAxis' rollover value is non-zero (i.e., ≥ 0 < PosAxis' Rollover Value)
  Unit user units
  Default n/a
Position Description The position the axis is set to when a good registration mark occurs.
  Data type LREAL
  Range When converted to feedback units, the range is: 
  • [-251,251-1] if PosAxis' rollover value is zero
  • [0, PosAxis' Rollover Value] if PosAxis' rollover value is non-zero (i.e., ≥ 0 < PosAxis' Rollover Value)
  Unit user units
  Default n/a
PosAxis Description The position of this axis at the time the fast input occurs is compared to the Target position to determine the amount of registration compensation to apply.
  Data type AXIS_REF
  Range The range of .AXIS_NUM is [1,256]
  Unit n/a
  Default n/a
CompAxis Description The calculated registration compensation is applied to this axis.
  Data type AXIS_REF
  Range The range of .AXIS_NUM is [1,256]
  Unit n/a
  Default n/a
PosTolerance Description This value specifies the distance, plus or minus, about the Target position to determine if the position will be accepted and compensation value is calculated and applied.
  Data type LREAL
  Range When converted to feedback units, the range is [-251,251-1]
  Unit user units
  Default n/a
RatioNumerator Description This value is typically the number of User Units of CompAxis motion for one product cycle. This value is used with RatioDenominator to create a conversion factor for calculating the compensation value when PosAxis and CompAxis are different axes.
  Data type DINT
  Range When converted to feedback units, the range is [1,4294967295]
  Unit user units
  Default n/a
RatioDenominator Description This value is typically the number of User Units of PosAxis motion for one product cycle. This value is used with RatioNumerator to create a conversion factor for calculating the compensation value when PosAxis and CompAxis are different axes.
  Data type DINT
  Range When converted to feedback units, the range is [1,4294967295]
  Unit user units
  Default n/a
Options Description Each bit enables/disables an option. The following table defines the bits. Any bits not defined are reserved. The third bit, 0004H, must be 0.
  Data type UINT
  Range refer to the following options table
  Unit n/a
  Default n/a
Hexadecimal Decimal Option Description
0001 H 1 Absolute/Resetting 0 = Resetting, 1 = Absolute
0002 H 2 Reserved 0
0004 H 4 Time/position based capture 0 = time based capture, 1 = position based capture
0008 H 8 Inhibit Reference on Good Mark 0 = Perform reference, 1 = inhibit reference
0010H 16 Inhibit Master Compensation 0 = Perform Master Compensation, 1 = Inhibit Master Compensation
0020H 32 Inhibit Slave Compensation 0 = Perform Slave Compensation, 1 = Inhibit Slave Compensation.

Table 11-44: MC_MachRegist Options Table

Outputs

RegistOn Description

Indicates registration is activated

  Data type

BOOL

Aborted Description Indicates registration has been terminated by MC_StopRegist.

 

Data type BOOL
Error Description Indicates an invalid input was specified or registration was terminated due to an error

 

Data type BOOL
ErrorID Description Indicates the error if Error output is TRUE. See table in PLCopen Function Block ErrorID Output.

 

Data type INT

Related Functions

MC_ReadParam

MC_StopRegist

MC_WriteParam

Examples

Function Block

Instruction List

Ladder Diagram

Structured Text

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™