You are here: Technical References > Motion Library > Motion/PLCopen > MC_MarkRegist

Function BlockMC_MarkRegistPLCopen motion icon

Description

This function block enables mark-to-mark registration and can be used on any servo or digitizing axis and with any move type. This function block is most frequently used in master/slave applications.

Used with ... Effect
Non-slave moves Resets the axis position when a good mark is captured by the fast inputThe inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action.
Slave moves In addition to resetting the axis position, applies a compensation offset to correct for the difference between the target mark-to-mark distance and the measured mark-to-mark distance. This provides the ability to compensate for product or process inconsistencies providing a system that remains synchronized with no accumulated error and maintaining repeatable accuracy throughout the process.

Arguments

Input

En

Description

Rising edge of EN enables execution
 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

Axis

Description

Axis to apply registration to
 

Data type

AXIS_REF
 

Range

The range of .AXIS_NUM is [1,256]
 

Unit

n/a
 

Default

n/a
TriggerInput

Description

Structure specifying the fast input.

The structure elements are:

InputID INT

0 = Capture Engine 0

1 = Capture Engine 1

Range is [0,1]

For information on configuring the capture engines, refer to AKD Capture Engine Configuration.

DirectionINT
1 = rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge, 2 = falling edge, 3 = NA, 4 = toggle between both, falling edge first, 5 = toggle between both, rising edge first, range = [1,5]

TrigIDINT
Axis number of the fast input. Zero indicates this trigger axis is to be the same as the Axis input. range = [0,256]


  • TrigMode INT (TriggerInput.TrigMode) is not presently supported by this function. The TriggerInput.Mode may be supported in a future software version.
 

Data type

TRIGGER_REF
 

Range

 
 

Unit

 
 

Default

 
Distance

Description

This is the expected distance between good marks. Along with Tolerance and Ignore, this value is used to determine if the mark detected by the fast input is a good mark.
 

Data type

LREAL
 

Range

When converted to feedback units, the range is [-251,251-1]. This value must have the same sign as Ignore.
 

Unit

user units
 

Default

n/a
Tolerance

Description

This value specifies the distance, plus or minus, about Distance to determine if the mark detected by the fast input is a good mark.
 

Data type

LREAL
 

Range

When converted to feedback units, the range is [0 ,251-1]
 

Unit

user units
 

Default

n/a
Ignore

Description

This value specifies the distance after the previous good mark in which any detected marks are ignored.
 

Data type

LREAL
 

Range

When converted to feedback units, the range is [-251,251-1]. This value must have the same sign as Distance.
 

Unit

user units
 

Default

n/a
Target

Description

This is the target distance between good marks. This distance is compared to the actual distance measured by the fast input to determine the amount of registration compensation to apply.
 

Data type

LREAL
 

Range

When converted to feedback units, the range is [-251,251-1]. This value must have the same sign as Distance.
 

Unit

user units
 

Default

n/a
Position

Description

The position the axis is set to when a good registration mark occurs
 

Data type

LREAL
 

Range

When converted to feedback units, the range is:

  • [-251,251-1] if PosAxis' rollover value is zero
  • [0, PosAxis' Rollover Value] if PosAxis' rollover value is non-zero (i.e., ≥ 0 < PosAxis' Rollover Value)
 

Unit

user units
 

Default

n/a
Options

Description

Each bit enables/disables an option. The following table defines the bits. Any bits not defined are reserved.
 

Data type

UINT
 

Range

Refer to the following options table.
 

Unit

n/a
 

Default

n/a
Hexadecimal Decimal Option Description
0001 H 1 Absolute/Resetting 0 = Resetting, 1 = Absolute
0002 H 2 Reserved 0
0004 H 4 Time/position based capture 0 = time based capture, 1 = position based capture
0008 H 8 Inhibit Reference on Good Mark 0 = Perform reference, 1 = inhibit reference
0010H 16 Inhibit Master Compensation 0 = Perform Master Compensation, 1 = Inhibit Master Compensation
0020H 32 Inhibit Slave Compensation 0 = Perform Slave Compensation, 1 = Inhibit Slave Compensation.

Table 11-45: MC_MarkRegist Options Table.

Outputs

RegistOn Description Indicates that registration is active.
  Data type

BOOL

Aborted Description Indicates registration has been terminated by MC_StopRegist.

 

Data type BOOL
Error Description Indicates an invalid input was specified or registration was terminated due to an error

 

Data type BOOL
ErrorID Description Indicates the error if Error output is TRUE. See table in PLCopen Function Block ErrorID Output.

 

Data type INT

Related Functions

MC_ReadParam

MC_Stop

MC_WriteParam

Examples

Function Block

Instruction List

Ladder Diagram

Structured Text

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™