You are here: Technical References > Motion Library > Motion/PLCopen > MC_MoveSuperimp

Function BlockMC_MoveSuperimpPLCopen motion icon

Description

This function block provides the ability to cause additional axis motion superimposed upon a currently executing move. A superimposed move is executed like an MC_MoveRelative move using the specified Distance, Velocity (i.e. VelocityDiff), Acceleration, Deceleration, and JerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time values. The interpolated command generated by a superimposed move is added to the command of the currently executing move. Subsequent calls to MC_MoveSuperimp can abort or blend to an executing MC_MoveSuperimp move.

This function block provides a way to smoothly apply a shift in axis position while it is executing a move.

MC_MoveSuperimp

Figure 11-137: MC_MoveSuperimp

Time Diagram

MC_MoveSuperimp: Timing Diagram

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

Execute Description Requests to queue the superimposed move
  Data type BOOL
  Range 0, 1
  Unit n/a
  Default —
Axis Description Name of a declared instance of the AXIS_REF library function. For more details, About Axis Name and Number
  Data type AXIS_REF
  Range [1,256]
  Unit n/a
  Default —
Distance Description Distance
  Data type LREAL
  Range —
  Unit User unit
  Default —
VelocityDiff Description Velocity rate
  Data type LREAL
  Range —
  Unit User unit/sec
  Default —
Acceleration Description Trapezoidal: Acceleration rate
S-curve: Maximum acceleration
  Data type LREAL
  Range —
  Unit User unit/sec2
  Default —
Deceleration Description Trapezoidal: Deceleration rate
S-curve: Unused
  Data type LREAL
  Range —
  Unit User unit/sec2
  Default —
Jerk Description Trapezoidal: 0
S-curve: Constant jerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time
  Data type LREAL
  Range —
  Unit User unit/sec3
  Default —
BufferMode Description
  1. abort
  2. buffer
  3. blend to active
  4. blend to next
  5. blend to low velocity
  6. blend to high velocity
See table in Buffer Modes
  Data type SINT
  Range [0,5]
  Unit n/a
  Default —

 

Output

Done Description

Indicates the move completed successfully.
The Command Position has reached the endpoint.

  Data type BOOL
Busy Description High from the moment the Execute input is one-shot to the time the move is ended
  Data type BOOL
Active Description Indicates this move is the active superimposed move
  Data type BOOL
CommandAborted Description Indicates the move was aborted
  Data type BOOL
Error Description Indicates an invalid input was specified or the move was terminated due to an error
  Data type BOOL
ErrorID Description Indicates the error if Error output is set to TRUE
See table in PLCopen Function Block ErrorID Output
  Data type INT

Example

Structured Text

(* MC_MoveSuperimp ST example *)
Inst_MC_MoveSuperimp( MovSupReq, Axis1, 123.555, 10.0, 100.0, 100.0, 0, 0 );
MovSupDone := Inst_MC_MoveSuperimp.Done; //store Done output into user defined variable

See also how this function is used in the Hole punch project here

Ladder Diagram

MC_MoveSuperimp: LD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™