You are here: Technical References > Motion Library > Motion/PLCopen > MC_Reference

Function BlockMC_ReferencePLCopen motion icon

Description

This function block is used to execute a fast home to a switch. If the application selects to reference to the index mark of an encoder, or the null of a resolver (which is typical), the new position value is assigned to the position of the index of the encoder (or the null of the resolver) and not the position of the switch. The ECATWriteSDO function block is used to setup the trigger event and any desired preconditions. This function block utilizes the Position Capture Mode of the AKD.

MC_Reference

Figure 11-150: MC_Reference

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

Execute Description Requests to queue the MC_Reference move and arms reference trigger events
  Data type BOOL
  Range 0, 1
  Unit n/a
  Default —

Axis

Description

Name of a declared instance of the AXIS_REF library function. For more details,About Axis Name and Number)

  Data type

AXIS_REF

  Range

[1,256]

  Unit

n/a

  Default

—

TriggerInput

Description

TRIGGER_REF structure defines the trigger

InputID INT :

0 = Capture Engine 0

1 = Capture Engine 1

Range is [0,1]

For information on configuring the capture engines, refer to AKD Capture Engine Configuration.

Direction INT; 1 = rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge of trigger, 2 = falling edge of trigger

Trigid INT; must be zero


  • TrigMode INT (TriggerInput.TrigMode) is not presently supported by this function. The TriggerInput.Mode may be supported in a future software version.
  Data type

TRIGGER_REF

  Range

See Description above

  Unit

n/a

  Default

—

Velocity

Description

Commanded velocity for the reference move

  Data type

LREAL

  Range

—

  Unit

User unit/sec

  Default

—

Acceleration Description Commanded acceleration for the reference move
  Data type LREAL
  Range —
  Unit User unit/sec2
  Default —
Deceleration Description Commanded deceleration for the reference move
  Data type LREAL
  Range —
  Unit User unit/sec2
  Default —
JerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time Description Commanded jerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time for the reference move (if zero, then trapezoidal acc/dec is used)
  Data type LREAL
  Range —
  Unit User unit/sec3
  Default —
Direction Description Commanded Direction of the reference
  Data type SINT
  Range [0,1]
  Unit n/a
  Default —
Position Description The position the axis will be reset to when at the machine reference location
  Data type LREAL
  Range —
  Unit User unit
  Default —
Option Description

Option identifier for Resolvers/Modulo reference.

0 = Use latched position for reference

1 = use resolver position of nearest null for reference 2 pole resolver

2 = use resolver position of nearest null for reference 4 pole resolver

3 = use resolver position of nearest null for reference 6 pole resolver

4 = use resolver position of nearest null for reference 8 pole resolver

5 = use resolver position of nearest null for reference 10 pole resolver

…

15 = use resolver position of nearest null for reference 30 pole resolver

  Data type SINT
  Range [0,15]
  Unit n/a
  Default —

Output

Done Description Indicates the reference move and position adjustment is complete
  Data type BOOL
Busy Description Indicates this function block is executing
  Data type BOOL
Active Description Indicates this move is the Active move
  Data type BOOL
CommandAborted Description Indicates the move was aborted
  Data type BOOL
Error Description Indicates an invalid input, or the move was terminated due to an error
  Data type BOOL
ErrorID Description

Indicates the error if the Error output is high

See table in PLCopen Function Block ErrorID Output

  Data type INT

Usage

The following lists the steps for homing a PLCopen axis, using the MC_Reference function block. Not all of the steps are necessary depending on the configuration and the homing cycle design.

The sequence of events of a PLCopen homing cycle consists of the following steps:

For more details, see "PLCopen Homing"

Related Functions

ECATWriteSdo

MC_MoveAbsolute

Example

Structured Text

 

(* MC_Reference ST example *)

TriggerInput.InputID := 0; //configure the reference InputID

TriggerInput.DIRECTION := 1; //configure the reference direction

Inst_MC_Reference( RefReq, Axis1, TriggerInput, 20.0, 100.0, 100.0, 100.0, 0, 0.0, 0 );

 

Ladder Diagram

MC_Reference: LD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™