You are here: Technical References > Motion Library > Motion/Pipe Network > MLPMPAbs

FunctionMLPmpAbsPipe Network motion icon

Description

Move to an Absolute Position using a parabolic acceleration profile. The FIRST_TRAVEL_SPEED is used as the velocity for the motion. JERK determines the level of parabolic acceleration. Returns TRUE if the function succeeded.

Arguments

Input

BlockID Description ID Name of the PMP function block in the Pipe Network
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit n/a
  Default —
Position Description Absolute Position of motor/load to be at after this FB is complete
  Data type LREAL
  Range —
  Unit User unit
  Default —

Output

Default (.Q)

Description Returns True if the function block is successfully executing

See more details here

  Data type BOOL
  Unit n/a

Related Functions

MLPmpWriteAccel

MLPmpWriteJerk

MLPmpWriteFstSpd

Example

Structured Text

 

MLPmpAbs( PipeNetwork.PmpMaster, 1000.0 ) ;

 

Ladder Diagram

MLPmpAbs: LD example

Function Block Diagram

MLPmpAbs: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™