You are here: Technical References > Motion Library > Motion/Pipe Network > MLPhaReadPhase

FunctionMLPhaReadPhasePipe Network motion icon

Description

Get the phase value of a phaser block.

Arguments

Input

BlockID

Description

ID Name of a Phaser function block in the Pipe Network

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

Output

Phase

Data type

LREAL

Example

Structured Text

 

PresentPhase := MLPhaReadPhase( PipeNetwork.PhaseAdjust );

 

Ladder Diagram

MLPhaReadPhase: LD example

 

Function Block Diagram

MLPhaReadPhase: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™