You are here: Technical References > Motion Library > Motion/Pipe Network > MLPipeAct

Motion Library - Pipe Network

Name

Description

Return type

MLPipeAct

Activates a pipe

BOOL

MLPipeAddBlock

Adds a Pipe Block to a pipe

BOOL

MLPipeCreate

Creates a new pipe object

None

MLPipeDeact

Deactivates a pipe

BOOL

FunctionMLPipeActPipe Network motion icon

Description

Activates a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block. The first ends with the first converter, and has a Gear Pipe Block to transform the input values from the Master. The second pipe ends with the second converter, and has a CAM Pipe Block to modify the input values from the Master.

Once a Pipe is activated then history on the values in the Pipe's Blocks are saved and updated each program cycle. A Converter object connected to a destination Axis object cannot send updated position values unless its Pipe is activated.

MLPipeAct

Figure 11-63: MLPipeAct

Arguments

Input

PipeID

Description

ID number of a created Pipe object

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe is activated

See more details here

 

Data type

BOOL

 

Unit

n/a

Return Type

BOOL

Related Functions

MLPipeDeact

MLCNVConnect

PipeNetwork(MLPN_ACTIVATE)

MLPipeAddBlock

Example

Structured Text

 

//Activate a Pipe

MLPipeAct( PipeAXIS1 );

 

Ladder Diagram

MLPipeAct: LD example

 

Function Block Diagram

MLPipeAct: FBD example

Go back to the top of the page [Top]

FunctionMLPipeAddBlockPipe Network motion icon

Description

Add a Pipe Block to a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between.

The figure below shows two Pipes, both with the same Master Input Pipe Block. If a user were to create the Pipe 1 below without using the Graphical Engine, they would use the following commands once a Pipe and the Pipe Blocks have been created.

MLPipeAddBlock( PipeAXIS1, MASTER);

MLPipeAddBlock( PipeAXIS1, MyGear);

MLPipeAddBlock( PipeAXIS1, CNV1);

MLPipeAddBlock

Figure 11-64: MLPipeAddBlock

Arguments

Input

PipeID

Description

ID number of a created Pipe

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

BlockID

Description

ID number of a created Pipe object to add to the selected Pipe

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe Block is added to the Pipe

See more details here

 

Data type

BOOL

 

Unit

n/a

Return Type

BOOL

Related Functions

PipeNetwork(MLPN_CREATE_OBJECTS)

MLPipeAct

MLPipeCreate

MLPipeDeact

Example

Structured Text

 

//Add a block to a pipe

MLPipeAddBlock( PipeAXIS1, MyGear );

 

Ladder Diagram

MLPipeAddBlock: LD example

 

Function Block Diagram

MLPipeAddBlock: FBD example

Go back to the top of the page [Top]

FunctionMLPipeCreatePipe Network motion icon

Description

Create a new pipe object. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block.

Arguments

Input

Name

Description

Desired name for the newly created Pipe

 

Data type

String

 

Range

—

 

Unit

n/a

 

Default

—

Output

ID

Description

Assigned ID number of the created Pipe

 

Data type

DINT

 

Unit

n/a

 

Default

—

Related Functions

PipeNetwork(MLPN_CREATE_OBJECTS)

MLPipeAddBlock

MLPipeAct

MLPipeDeact

Example

Structured Text

 

//Create a new pipe

PipeAXIS1 := MLPipeCreate( 'PipeAXIS1' );

 

Ladder Diagram

MLPipeCreate: LD example

 

Function Block Diagram

MLPipeCreate: FBD example

Go back to the top of the page [Top]

FunctionMLPipeDeactPipe Network motion icon

Description

Deactivates a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block. The first ends with the first converter, and has a Gear Pipe Block to transform the input values from the Master. The second pipe ends with the second converter, and has a CAM Pipe Block to modify the input values from the Master.

Once a Pipe is activated then history on the values in the Pipe's Blocks are lost and no longer updated. A Converter object connected to a destination Axis object cannot send updated position values once its Pipe is deactivated.

MLPipeDeact

Figure 11-65: MLPipeDeact

Arguments

Input

PipeID

Description

ID number of a created Pipe object

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe is deactivated

See more details here

 

Data type

BOOL

 

Unit

n/a

Return Type

BOOL

Related Functions

MLPipeAct

MLCNVDisconnect

PipeNetwork(MLPN_DEACTIVATE)

MLPipeAddBlock

Example

Structured Text

 

//Deactivate a Pipe

MLPipeDeact( PipeAXIS1 );

 

Ladder Diagram

MLPipeDeact: LD example

Function Block Diagram

MLPipeDeact: FBD example

Go back to the top of the page [Top]

 

MLPipeAct

MLPipeAddBlock

MLPipeCreate

MLPipeDeact


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™