You are here: Technical References > Programming Languages > PLC Standard Libraries > udpRcvFromVar

FunctionudpRcvFromVarPLCopen motion icon

Description

This function receives the contents a variable sent from another controller and saves it to a local variable. This allows for the exchange of data across controllers.

Arguments

Input

En Description Execute the function
  Data type BOOL
  Range [0,1]
  Unit n/a
  Default —
sock Description Socket number, return value from udpCreate
  Data type DINT
  Range [0,+65535]
  Unit n/a
  Default —
add[] Description Array which contains information about the server
  Data type USINT
  Range [0,32]
  Unit n/a
  Default —
varName Description The name of a variable to save the data received from the sender. The variable should be the same type as what is being sent. See udpSendToVar.
  Data type STRING
  Range  
  Unit n/a
  Default —

Output

OK Description Returns true when the function successfully executes. See Function - General rules.
  Data type BOOL
  Unit n/a
Q Description Number of bytes received
  Data type DINT
  Unit n/a

Examples

Structured Text

udpRcvFromVar( Socket_Number, Add, MyUDPVar )

Ladder Diagram

Function Block Diagram

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™