| HMI
|
|
At the end-user top level, the Human Interface is where the operator can monitor or operate the system. It is usually composed of a panel on a . |
| Communication
|
|
is linked to the middle layer via a non time critical communication system (e.g. TCP protocol on ). |
| PLC
|
|
Programmable Logic Controllers is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. It is used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to and events. |
| Motion Engine
|
|
There are two Motion Engines available: Pipe Network and PLCopen. The Motion Engine implements different motion algorithms and functions to create, access and delete pipes, pipe blocks and axes. It also provides a set of Functions and Function Blocks that 61131-3 applications can use to control the behavior of these algorithms. |
| Fieldbus
|
|
The fieldbus is the way to connect instruments in a plant design by linking the to the external systems. |
| I/O
|
|
Input/Output refers to the communication between your automation system, and the outside world. |
| Drive
|
|
A is an electronic device that provides power to a motor or servo. |
| Motor
|
|
At the bottom of the control chain is the motor which actually does the work. |