The rotary switch on the PDMM or PCMM can be set on a position from 0 to 9.
| Switch Position | Description |
|---|---|
| Position 0 | The drive tries to get an IP address from a DHCP server. If the DHCP fails, then the PDMM or PCMM uses AutoIP to get a usable IP address. |
| Position 1 | The default custom static IP address, 192.168.0.101 or a custom IP address. |
| Position 2-9 | The PDMM or PCMM is pre-configured with static IP addresses ranging from 192.168.0.102 (Position 2) to 192.168.0.109 (Position 9). |
If a DHCP server is not present, the drive will assume an Automatic Private IP Address of the form 169.254.x.x
The PDMM or PCMM will not set (or show) an IP address without an attached network cable.
|
Copyright © 2015 Kollmorgen™ |
|