You are here: Understanding KAS > EtherCAT Motion Bus Concepts > CANopen > CANopen Status Machine

CANopen Status Machine

The states of the status machine can be revealed by using the CANopen Status Word.

CANopen Status Machine

Figure 5-62: CANopen Status Machine

The start state is a pseudo-state indicating the start when the state machine is activated during the start-up sequence of the device drive's application software.

Status description

Status Description
Not ready to switch on The drive is not ready to switch on. The controller has not indicated readiness for service. The drive is still in the boot phase or in the fault status
Switch on disabled The drive cannot be enabled via the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs interface; because for example there is no connection to a power source
Ready to switch on The drive can be enabled via the control word. DC-link voltage can be switched on, parameters can be transferred, motion functions cannot be performed yet.
Switched on The drive is enabled but the setpoints are not yet transferred from the EtherCAT interface. The drive is idle. DC-link voltage must be switched on, parameters can be transferred, but motion functions cannot be performed yet. Output stage is switched on (enabled). Operation EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. No fault present; output stage is enabled; motion functions are enabled.
Operation enabled The drive is enabled and the setpoints are transferred from the EtherCAT interface. No fault present; output stage is enabled; motion functions are enabled.
Quick stop active The drive has been stopped with the quick stop ramp; output stage is enabled; motion functions are not enabled.
Fault reaction active A fault has occurred and the drive is stopped with the emergency stop ramp
Fault A fault is active, and the drive has been stopped and disabled

Table 5-5: Status Description

Transitions of the status machine

The drive device supports the transitions and actions as listed in the table below. The event initiates the transition. The transition is terminated after the action has been performed.

Transition Event Action
0 Automatic transition after power-on or reset application DriveControl device for regulating the speed, torque and position of a motor device self-test and/or self initialization has to be performed.
1 Automatic transition Communication has to be activated.
2 Shutdown command from control device or local signal None

3

Switch on command received from control device or local signal

The high-level power has to be switched on, if possible.

4

Enable operation command received from control device or local signal

The drive function has to be enabled and all internal setpoints cleared.

5

DisableRemoval of the ENABLE signal. Disables power stage. operation command received from control device or local signal

The drive function has to be disabled.

6

Shutdown command received from control device or local signal

The high-level power has to be switched off, if possible.

7

Quick stop or disable voltage command from control device or local signal

None

8

Shutdown command from control device or local signal

The drive function has to be disabled, and the high-level power has to be switched off, if possible.

9

Disable voltage command from control device or local signal

The drive function has to be disabled, and the high-level power has to be switched off, if possible.

10

Disable voltage or quick stop command from control device or local signal

The high-level power has to be switched off, if possible.

11

Quick stop command from control device or local signal

The quick stop function has to be started.

12

Automatic transition when the quick stop function is completed and quick stop option code is 1, 2, 3 or 4, or disable voltage command received from control device (depends on the quick stop option code)

The drive function has to be disabled, and the high-level power has to be switched off, if possible.

13

Fault signal

The configured fault reaction function has to be executed.

14

Automatic transition

The drive function has to be disabled; the high-level power has to be switched off, if possible.

15

Fault reset command from control device or local signal

A reset of the fault condition is performed, if no fault exists currently on the drive device; after leaving the Fault state, the Fault reset bit in the control word has to be cleared by the control device.

16

Enable operation command from control device, if the quick stop option code is 5, 6, 7, or 8

The drive function has to be enabled.

Table 5-6: Transition Events and Actions

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™