You are here: Understanding KAS > Motion Concepts > PLCopen > Behavior of CommandAborted Output

Behavior of CommandAborted Output

CommandAborted is set when a commanded motion is interrupted by another motion command.
The reset-behavior of CommandAborted is like that of Done. When CommandAborted occurs, the other output signals such as InVelocity are reset.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™