You are here: Understanding KAS > Motion Concepts > PLCopen > Error Handling Behavior

Error Handling Behavior

Two outputs deal with errors that can occur while executing a function block. These outputs are defined as follows:

Done, InVelocity, InGear, and InSync mean successful completion so these signals are logically exclusive to Error.
Instance errors do not always result in an axis error. Some bring the axis to StandStill(see "State machine" for more details).

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™