You are here: Understanding KAS > Motion Concepts > PLCopen > Input Parameters

Input parameters

Unless specified otherwise in the function block's description, the input parameters are read with the rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge of the Execute input.

The input parameters can be as follows:

For the list of input parameters and its description for PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Function/Function Blocks, see "List of Input Parameters"

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™