You are here: Understanding KAS > Motion Concepts > PLCopen > Output 'Active'

Output 'Active'

The Active output is set at the moment the function block takes control of the motion of the respective axis.

Coordinated Motion

Use the following table to determine the state of the Busy and Active outputs when transitioning from one move to the next.

Function Block Output First Move Second Move
Busy False True
Active False False
Done True1This output will be false if the move is interrupted by a MC_GrpHalt, MC_GrpStop, or if the second move's buffer mode is "Aborting". False

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™