You are here: Understanding KAS > Motion Concepts > PLCopen > Output Exclusivity

Output Exclusivity

If the Execute input of a function block is set TRUE, either the Busy, Done, Error, or CommandAborted outputs must also be set TRUE. These outputs are mutually exclusive, meaning that a function block may have only one of them set TRUE at any time.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™