To create the Pipe Network, do as follows:

Figure 4-6: Pipe Network - Open Editor
If you have created a project from a template (for instance the standard two-axis template) there is already a Pipe Network in the editor.

Figure 4-7: Pipe Network - Add Pipeblock
For more details on Pipe Blocks, refer to Pipe Block and Pipe Blocks Description

Right-click on the Pipe Block and select the Delete command in the contextual menu.
You can either:
See also §O.3: Application Notes for application examples
|
Copyright © 2015 Kollmorgen™ |
|