You are here: Getting Started > Creating a Project > Step 4 - Adding Motion > Set the Position Units

Set the Position Units

You can set up the position units in the parameter screen of the Axis block.

Setting Axis Units

Figure 4-14: Setting Axis Units

Some guidelines for suitable settings advises for a good choice is given below:

Setting the Units - Example

Figure 4-15: Setting the Units - Example

A User Unit = 0.1mm could be selected for this transportation system

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™