It is possible that after a Controller RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running upgrade that the Runtime and the compiled project versions major.minor.micro may be different. The Runtime will not start if there is an incompatibility between the versions.
| PDMM or PCMM | An E24 error will be displayed and an error will be logged if compiled project version is incompatible with the Runtime version. |
| PAC | An error will be logged if the compiled project version is incompatible with the Runtime version. |
To correct the incompatible versions, either re-compile and download the KAS project file using the same IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger version as the Runtime version OR change the Controller's Runtime version to match the compiled project's version.
|
Copyright © 2015 Kollmorgen™ |
|