You are here: KAS IDE Reference > EtherCAT Devices > Select Input and Output PDOs

PDO Selection/Mapping Tab

This tab includes the PDO configurations for an EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs device.

The assigned PDOs and their objects are viewable for the Inputs (Tx) and Outputs (Rx). The PDOs become active when the EtherCAT network is initialized to operation mode.

Each assigned PDO is listed by its Index (hex) and Name. The objects associated with each PDO are listed below the name. The objects are identified by their object dictionary Index and Subindex. The Object Name provides a simple description. The Size determines the data length. The PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Variable mapped to the PDO objects is also listed.

Select Input and Output PDOs

Press the Select Input (Tx) PDOs or Select Output (Rx) PDOs button to choose the Input or Output PDOs. The appropriate dialog box will open.

(S300"Servostar 300 drive" See Servo Drive in Glossary/700 content)

Viewing the contents of a PDO

Click on a row in the upper portion of the PDO Selector dialog box to view the contents of that PDO. The lower portion will update to list the associated objects. Using the following example, the PDOs 0x1A02 and 0x1A03 are selected for the input objects but the contents for PDO 0x1A00 are listed because that row is selected..

  1. Selected PDOs
  2. Selected row
  3. Contents of selected row's PDO.
 

Map PLC Variable to PDO Object

PLC variables can be mapped to PDO objects by:

For more details, please see Map Input and Output to Variables.

 

Select Input and Output PDOs

Viewing the contents of a PDO

Map PLC variables to a PDO object


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™