| Automatic Mode | The boot from the recovery image is done automatically if the regular image is corrupted. |
| Manual Mode |
If the controller starts booting normally but freezes after the startup script (see image to the right), then you have to boot manually from the recovery image by pressing the recovery button (B2). See Booting from the Recovery Image for more information. |
The controller will display a "backward C" on the 7-segment display if the wrong firmware is installed. You must enter recovery mode to load the correct firmware file.
|
Copyright © 2015 Kollmorgen™ |
|