You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Webserver Import Export Tab

Import/Export

These functions allow you to save a copy of the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs configurations backup file to a computer and Import the backup file so it may be used for restore functions.

Export Backup This button allows you to save a backup of the EtherCAT configuration to a computer.
Choose File This button allows you to select a previously exported backup file to be imported.
Replace Backup This button imports the selected backup file, replacing any existing backup.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™