You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Axis

Axis

You can view a visual representation of the motors from the Axis tab. The axis wheels are visible after your application is started. The following can be monitored from the display: 

Information that is available by clicking on the axis
Title Image (PN axis) Image (PLCopen axis) Image (digitizing axis)

See theAxis Pipe Block section of the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger documentation for information about the axis parameters.

See Axis Parameters in the PLCopen Function Blocks - Overview section of the KAS IDE documentation for information about the axis parameters.

Additionally, if an axis is in error, the error can be cleared by clicking the text below the axis title.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™