You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Log Message Content

Log Data

KAS log files may be viewed from the Log Data tab. These messages can help describe the current state of the system and to help identify any operation errors encountered when developing your system. A PDMM or PCMM will display as many as 10 files.

Figure 7-2: Example of log files displayed from a PDMM or PCMM webserver.

Clicking on a listed log file will open it in your web browser. The log file may be downloaded by clicking on the green download icon next to the log entry. The default name is the same as the file's name. If you try to open a file that no longer exists, the message "/logfiles/<selected file name> not found." Refresh your browser window and try again.

Figure 7-3: Example of a log file's content, displayed in a browser.

Log Message Content

Every log message in the table has the following information:

Field

Description

Time

Time when the log was recorded with the format:
DD-MMMM-YY hh:mm:ss (millisecond)

Source

Identifies a software or hardware component issuing the messages. Each source is configured with a specific Level.

Level

Each message has one of the following levels with importance in ascending order:
DEBUG > INFO > WARNING > ERROR > CRITICAL

Message

Text of the message issued from the source

Table 7-5: Log Messages - List of Field

 

Log Message Content

PDMM and PCMM Log Files

PAC Log Files


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™