You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > User Data

User Data

This tab lists any user-generated files or folders found in the PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system's compact flash drive, PDMM's, or PCMM's flash memory. Clicking a folder will display the folders contents. Clicking on the green download icon will immediately download the file.

The Clear User Data button will erase all of the files in the user data folder.

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™