You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Reset the Control to Factory Settings

File System Tab

This section contains a button which allows you to reset the control to the factory settings. The steps to reset the controller vary slightly based on the platform.

  1. PDMMor PCMM
  2. PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system
  3. Simulator

Figure 7-5: File System tab on an PDMM or PCMM web server, PAC web server, and when using Simulator.

Reset to Factory Settings

When this button is pressed, the control will be reset to factory default settings. The user is prompted to confirm this action before the function is performed.

The following changes occur during factory reset:

‡ PDMM and PCMM only

Notes about the reset:

 

Reset the Control to Factory Settings


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™