You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Change the IP Address

Network Tab (PDMM or PCMM Only)

The contents of this tab display the current rotary switch position of the PDMM or PCMM and its MAC addressA Media Access Control address (MAC address) is a quasi-unique identifier assigned to most network adapters or network interface cards (NICs) by the manufacturer for identification. If assigned by the manufacturer, a MAC address usually encodes the manufacturer's registered identification number. Additionally, you may manually change the AKD PDMM's or PCMM's IP address.

Figure 7-4: Example of a PDMM or PCMM with a manually defined IP address

About the Rotary Switch

The rotary switch on the PDMM or PCMM can be set on a position from 0 to 9.

Switch Position Description
Position 0 The drive tries to get an IP address from a DHCP server. If the DHCP fails, then the PDMM or PCMM uses AutoIP to get a usable IP address.
Position 1 The default custom static IP address, 192.168.0.101 or a custom IP address.
Position 2-9 The PDMM or PCMM is pre-configured with static IP addresses ranging from 192.168.0.102 (Position 2) to 192.168.0.109 (Position 9).

Change the IP Address

To connect and use your PDMM or PCMM within your computer network, you may configure its IP address by using the web server as follows:

  1. Open the controller's web server in your internet browser
  2. Select the Settings tabbed-page
  3. In the Network pane, set static IP address according to the position defined via the rotary switch
  4. Configure the Manual IP Address
  5. Configure the subnet mask (default is 255.255.255.0)
  6. (Optional) Configure the gateway address if the PDMM or PCMM is outside your local network
  7. Click Apply
  8. Click Reboot

 

Change the IP Address

About the Rotary Switch


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™