You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > Security

Security

Some parts of the web server are locked in order to protect critical operations from unauthorized users. Simply log into the web server to enable access to the locked functions. See User Authentication for more information.

The functions which are locked are:

‡ PDMM and PCMM only

 

Timeout After Inactivity


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™