You are here: Tools > Human Machine Interface Editor > Using the Internal Editor > Create Control Panel

Create Control Panel

Control Panel are managed in the Project Explorer and can be created as follows:

  1. In the Project Explorer, right-click the Controller item to open the menu
  2. Select the New Control Panel command
  3. Right-click on the newly created item and select the Rename command to change its name
  4. Double-click the new Control Panel to open it in the graphical editor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™