You are here: Tools > AKD into KAS > PDMM Firmware > Download AKD PDMM Drive Firmware

Download AKD PDMM Drive Firmware

Component Firmware Version Download
800MHz PDMM DriveControl device for regulating the speed, torque and position of a motor FW AKD-M-MCEC-V1.15-00-003.i00
1.2GHz PDMM Drive FW AKD-M-M1EC-V1.15-00-003.i00

To upgrade PDMM drive Firmware with KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger, continue from the previous procedure as follows:

  1. In the toolbar, deactivate the Online Configuration Mode
  2. Select the drives requiring the same firmware version to be updated
    (Note that the FW download is limited to 16 drives at a time)
  3. Click Upgrade Firmware button
  4. Browse to select the new AKD firmware file
  5. Click Open to start the updating procedure

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™