You are here: Tools > AKD into KAS > PDMM Firmware > AKD Firmware Update

AKD Firmware Update

Based on the File Access over EtherCAT (FoE) protocol, the AKD drive Firmware can be downloaded as follows:

  1. Scan the devices and make sure all devices are created
  2. Compile the project
  3. Connect to the controller
  4. Download the project to the controller
  5. Open the EtherCAT Devices summary form
  6. Select the drives requiring the same firmware version to be updated
  7. Click the Upgrade Firmware button
  8. Browse to select the new AKD firmware file matching the AKD revision. Refer to the Release Notes for the latest supported firmware.
  9. Click Open to start the updating procedure

During the firmware download, the AKD Firmware Update window displays a progress bar and the following messages are displayed:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™