You are here: Tools > Softscope > Probes

Plugging Probes

A probe is a virtual measurement point that can be connected to a variable.

Three types of variables can be plugged:

  1. Pipe Block variable which is a Pipe Block related variable.
  2. IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 variable which is any other variable.
  3. PLCOpen axis values.

You can connect a probe to a variable in one of the following ways:

 

Plug in Softscope

Plug in Dictionary

Plug in Pipe Network


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™