You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Dictionary > Enum tab

Enum Tab

This tab allows you to define enums (Enumerated Types). An enumerated type allows you to define a data type and assign a specific set of accepted values.

Adding Enums

An enum may be created in one of two ways:

This creates a default enum labelled as "EnumTypen" with the Value of "V0,V1".

Double click on the Type or Value to make changes.

To Use Enums

  1. Enter the enum type and hash (#), the press Ctrl+Space. This opens a dialog to select the corresponding value.
  2. Select the value and click the check mark. The value is loaded into your program.

Declaring Enums

Enums may be declared in the same way as variables; at the end of the line press Enter.

As CurrentDrive is not a part of the dictionary, a dialog is opened to add the variable. Set the Types as the enum name.

Once this is added, the variable will be displayed with the selected type in the Dictionary.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™