You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Information and Logs > Browse Variable

Browse Variable Tab

This tab is used to browse all instances of a variable. It will show the locations and usage of each instance of a single variable. There are two ways to populate the tab:

Using the Browse Variable tab

  1. Click the Select Variable button to open a variable selection pop-up window.
  2. Select a variable from the pop-up list.
  3. The Browse Variable tab is updated with a two-column table detailing the variable's usage
  4. Double-click on an entry to be taken to the correspondinglocation in the editor.

Using the Dictionary's Browse Variable menu item

The first time this menu is accessed (per project instance) you are presented with Update browse info. This updates the browse data. Further selections of any variable result in the location and usage being shown directly in the menu.

When the menu has more than ten entries an ellipsis (…) is added to the bottom of the menu.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™